NTN Europe launches ROX: the bearing designed to reduce maintenance downtime on conveyors in quarries and mines
- France - Industry OEM - Products
ROX - BORN FOR THE DUST.
ROX is the only spherical roller bearing in the world equipped with two patented metal deflectors, designed to effectively block the entry of dust and debris, while its nitrided cage reinforces resistance to impact and harsh conditions.
Developed for maintenance managers, ROX significantly reduces maintenance frequency, lowers downtime costs, and limits environmental impact.
With ROX, bearing life is increased by more than 2 times, lubrication is reduced by more than 50%, while remaining 100% compatible with standard premium (ISO) bearings.
Designed to last, ROX operates from -40°C to +200°C and accepts up to 2° of misalignment.
It is positioned as the benchmark solution for conveyor applications in dusty and extreme environments: quarries, cement plants, mines, cardboard factories... wherever continuity of service and reliability are key issues.
With ROX from SNR brand, NTN Europe supports its customers over the long term, offering them innovative technologies that are increasingly robust, high-performance, and adapted to the realities of the field.
NTN is renewing its support for the rally team Sarah Rumeau and Julie Amblard in 2026!
- France - Corporate - Organisation
The adventure continues! NTN is proud to renew its partnership with the all-female duo comprising Sarah Rumeau and Julie Amblardfor the 2026 season. A year that promises to be one of renewal and transformation, featuring: a new car, a new team and new objectives. A new chapter… Read more
NTN Europe launches MySNR CertifiedGarage: a platform entirely dedicated to garage owners
- France - Automotive Aftermarket - Services
It's official! NTN Europe is launching MySNR CertifiedGarage in France, a new digital platform dedicated entirely to garage owners, designed to simplify their daily operation and optimise the management of their workshops. This exclusive solution marks a new step in strengthening NTN Europe'… Read more