The voice of the Experts

Our publications

Welcome to the NTN's blog. Our experts speak on subjects
related to automobile, industry, innovation, company's life...

10 Nov 2023

A particularly harsh environment Here is what an on-site storage area for rollers and bearings can sometimes look like. Even if they don't all look like that, mines, qua...

22 Dec 2022

A rolling bearing is a bearing which carries a load by placing rolling elements (such as balls or rollers) between two bearing rings called races. Behind the apparent st...

23 Feb 2022

There are many types of bearings, the most common being ball bearings, or tapered roller bearings, cylindrical or spherical roller bearings. Their design meets specific t...

16 Feb 2022

A tracked hydraulic excavator requires about fifty bearings for its basic operation (travel and rotation). Irrespective of its size and its use (earthwork, mining, demoli...

09 Feb 2022

WEC is an unusual failure of the bearing surface characterized by a network of branched white cracks (White Etching Cracks). The material is weakened, specifically by the...

02 Feb 2022

There’s an old saying: “no crops without fields, no wheat without manure”. But what is the real nature of this cultivated earth that towed agricultural machines turn, loo...