THE LATEST NTN INNOVATIONS

Discover the latest NTN innovations in the automotive, aerospace, robotics, electric vehicles and other industries...

NTN acts to meet challenges facing the industry. These examples of innovation illustrate the developments that we have carried out. They have addressed constraints and increased performance (technical or related to megatrends).

During the Automotive TechDays event, the international technical day of the Auvergne Rhône Alpes region Automotive and Transport competitiveness pole, organized by the Cluster Cara, the NTN innovation team had the opportunity to present the Compact wheel bearing and the Sustainable strut bearings:

Hybrid and electric vehicles require new constraints in terms of architecture of the running gear, as a result of the increased axle weight and the axial dimensions of the motor and gearbox assembly. Aware of these specific constraints to hybrid and electric vehicles, NTN, the world’s leading manufacturer of wheel bearings and homokinetic transmission joints, is currently working on the design of a new wheel bearing and transmission joint assembly that is more compact axially. The new design makes it possible to save up to 35mm in width per wheel, without reducing the service life assembly.

NTN Europe has developed an innovative concept of suspension bearings combining a recycled and recyclable aluminium support and a recycled plastic top-cover. 

The choice of aluminium increases the rigidity of the support and prolongs its life under severe conditions of stress, while providing a significant reduction in mass for an equivalent or even superior performance. The fine selection of high quality recycled polyamides guarantees technical performance that meets customer specifications. 

This combination, based on materials’ circular economy and perfectly aligned with the EU objectives to reduce the consumption of non-renewable resources, makes it possible to significantly decrease the associated environmental impact, with a gain in CO2 emissions of up to 4.8 kg eq. CO2 per vehicle (cradle-to-grave scope). 

This sustainable bearing has now reached a sufficient level of technical maturity to consider an industrial development during 2023 with a view to marketing by 2025.

ntn-snr-galet-tendeur-hydraulique

NTN has created hydraulic accessories belt tensioner roller with a variable shock-absorption mechanism for engines using the ISG (Integrated Starter Generator) Stop & Start function. This new solution, which allows for varied shock absorption using a dual-oil-passage, automatically adjusts the tension idler’s tension level to optimum settings which respond to the engine’s running conditions. Conventional tension idlers are unable to do this.

The NTN automatic tensioner with variable damping mechanism provides major improvements:

  • a significant drop in fuel consumption and CO2 reductions as a result of reduced friction at constant speed.
  • an increase in the useful life of the auxiliary components as a result of the constantly adjusting belt tension.
  • reliability guaranteed to be identical to the current systems.


 

NTN is committed to developing innovative solutions for the diagnosis of rotating machinery. We have developed sensors, enclosures and electronic software for preventive maintenance that monitor a full fleet of production machines and detect their signs of weaknesses. What are the advantages?

  • Reduced instrumentation costs
  • Easy integration to the existing equipment of operators
  • 100% integration to a new OEM product under development
outils-de-diagnostic-pour-maintenance-preventive
magnetoresistance-a-effet-tunnel

Developed in partnership with Sensitec, TMR is a new generation of magneto-resistance following in the footsteps of AMR and GMR. NTN has introduced a new sensing unit into the sensors, allowing better detection:

  • high precision
  • low energy consumption
  • higher airgap tolerances

NTN can offer a new type of cage with reverse positioning of tapered roller collars for gearbox applications or wheel bearings. This tapered bearing architecture, called reverse architecture, offers several advantages:

  • reduction of frictional losses
  • improved service life in low lubrication conditions
  • reduced axial dimensions
  • better discharge of thermal units

In the case of tapered unit wheel bearings, the risk of losing the wheel through an internal seizure is strongly reduced.

cage-avec-positionnement-inverse-des-rouleaux-coniques
entretoise-nouvelle-generation

In order to combine rotational speed requirements and increased reliability for machine tool applications, NTN offers a new generation spacer. Its design allows:

  • an ideal air flow
  • reduced consumption of fresh air
  • less noise
  • more homogeneous temperatures
  • the ability to run faster

The goods-producing industry is changing. In the field of robotics applications, NTN innovates by offering bearings that are optimised for cheaper and faster cobots:

  • up to 60% lighter
  • increased useful mass of a robot by 10% to 30%
  • overall downsizing

The maximum benefit is achieved when control of the cobot is made using a camera and NTN bearings incorporate the measurement of the position of each joint.

roulements-alleges
roulements-a-rotules-sur-rouleaux-proteges

Until now, using a spherical bearing in applications with polluted environments needed a choice to be made between either:

  • an open bearing, but one able to rotate fast and at high temperatures
  • a sealed bearing, which was wider and limited in terms of speed and temperature.

NTN offers a compromise: a spherical bearing protected from external particles, but able to rotate faster without needing to be wider. 
Other benefits: substantial cost reduction and fewer maintenance operations.

NTN is heavily involved in aerospace applications. Its hybrid bearings provide solutions in terms of:

  •  weight saving
  • reduction of centrifugal force
  • better resistance to the environment
  • good behaviour in the absence of lubrication
  • reduction in dissipated energy
  • increase in rotational speed

To ensure robustness and reliability of the hybrid bearing, NTN focuses on materials, non-destructive testing (NDT) and performance.

roulements-hybrides
roulements-a-rouleaux-coniques-haute-vitesse

NTN has developed high-speed tapered roller bearing solutions for engines and transmissions in aerospace applications. These bearings are associated with designs that are more resistant to oil loss.

NTN supports car manufacturers to prepare for the future and make cleaner cars. The 208 Hybrid FE prototype from PSA and the Eolab prototype from Renault can display record consumption of 2l/100 km and 1l/100km. They are fitted with NTN-SNR wheel and transmission bearings.

Technological innovations implemented by NTN have resulted in:

  • weight saving
  • reduction of frictional losses
  • reduction of emissions from 1.1 to 2.8 g of CO2/km
roulements-de-roue
actionneur-boite-de-vitesse

Cars offer increasingly complex features. This evolution in automotive applications requires components that incorporate more and more functions.

To support this trend, NTN has developed, among other systems, a gearbox actuator equipped with ball screws, an absolute position sensor (true power-on), electronics and control software.

This solution results in:

  • extremely precise positioning
  • a very compact system
  • reduction of frictional losses

Looking to the future of the automobile, NTN has developed an electric traction motor housed in the wheel. Of particular interest for small electric cars and hybrid utility vehicles, there are various advantages to this wheel motor:

  • freeing up of space in the chassis
  • optimisation of the vehicle dynamic behaviour
  • easier integration of the electric traction chain
  • unrivalled compactness by using a cycloid type gearbox
  • conservation of the conventional braking system

E-Wazuma is a demonstration prototype, produced in collaboration with Lazareth (Annecy, France), who specialise in recreational, unique and extraordinary vehicles.

moteur-roue-e-wazuma
roulement-de-rotor-ouvert

NTN is working on solutions intended for the next generation of more environmentally friendly aircraft engines. We have developed, among others, open rotor bearings under the CLEANSKY project. These integrated bearings provide solutions to meet the technical challenges of these new engines.

Complete your knowledge on NTN-SNR innovation. Learn more about our focus areas on materials, mechatronics.  See our product offer

Why don’t you innovate with us? CONTACT US