Mai jos veți găsi comunicatele și dosarele de presă ale NTN în Europa privind structura acesteia, produsele, serviciile, tehnologiile, inovațiile sale etc.
Presă
NTN-SNR is reinforcing its development in the offshore sector, and is expanding its onshore wind turbine activities
NTN-SNR will take part in the WindEnergy trade fair in Hamburg from 27 to 30 September 2016, where it will be showcasing its bearings designed for both onshore and offshore wind turbines. NTN-SNR...
Press kit: Automechanika Frankfurt - From 13th to 17th September 2016
At the Automechanika 2016 trade fair, which will run from 13th to 17th September 2016 in Frankfurt, NTN-SNR is launching two new ranges: a range of constantvelocity (CV) joint kits intended for...
NTN-SNR innove : Des joints de transmission et des roulements de boîtes de vitesses seront lancés a Automechanika !
À l’occasion du salon Automechanika 2016 qui se tiendra du 13 au 17 septembre 2016 à Francfort, NTN-SNR lance deux nouvelles gammes : une gamme de kits de transmission destinés au parc européen et...
The NTN-SNR Polipump has a good track record with Véolia
Since its launch in 2012, the NTN-SNR Polipump has been a real success. This multipoint unit offers up to 35 lubricating points with a pressure of 80 bar per point and easy and efficient...
NTN-SNR have developed a wireless position-measuring system for their linear modules
NTN-SNR have developed a linear module featuring a wireless position-measuring sensor built into the linear guidance system. Its compactness, ease of implementation and lack of wires make it a...
NTN-SNR's wide product range, modularity and innovations cover all automated movement needs
For the first time, NTN-SNR shall take part in Automatica, the international trade fair for robotics, automation and mechatronics to be held from 21 to 24 June in Munich. NTN-SNR is a major player...
NTN-SNR is ISO 50001 certified for all its French sites
In January 2016 NTN-SNR obtained ISO 50001 certification for energy efficiency for all its sites in France. The certification acknowledges the work done for several years on reducing NTN-SNR's...
NTN-SNR extends its lubrication range designed for the single-point lubrication system Ready Booster
NTN-SNR launches Food Chain Oil, its new food-grade oil designed specifically to meet demand from the food-processing and pharmaceutical industries. Food Chain Oil is intended for use with NTN-SNR...
NTN-SNR is launching in Europe the BBPS 10-100, its kit for extracting deep-groove ball bearings
NTN-SNR is launching in all of its European markets the BBPS 10-100, a kit for extracting deepgroove ball bearings, in order to meet demand for rapid and easy removal of bearings without the risk...
NTN-SNR deploys 2 flagship products for towed agricultural machines
After their launch at the end of last year, NTN-SNR is deploying its offering of built-in hubs and inserts for self-aligning bearing units for all manufacturers of agricultural machines and...