Presse

Nachfolgend finden Sie Pressemitteilungen und Pressemappen von NTN in Europa mit Informationen zu Organisationsstrukturen, Produkten, Dienstleistungen, Technologien und unseren Innovationen.

Alle Ergebnisse
pressrelease
September 2016 - Märkte

NTN-SNR innove : Des joints de transmission et des roulements de boîtes de vitesses seront lancés a Automechanika !

À l’occasion du salon Automechanika 2016 qui se tiendra du 13 au 17 septembre 2016 à Francfort, NTN-SNR lance deux nouvelles gammes : une gamme de kits de transmission destinés au parc européen et…

Lesen Sie den Artikel:
pressrelease
July 2016 - Gruppe

The NTN-SNR Polipump has a good track record with Véolia

Since its launch in 2012, the NTN-SNR Polipump has been a real success. This multipoint unit offers up to 35 lubricating points with a pressure of 80 bar per point and easy and efficient…

Lesen Sie den Artikel:
pressrelease
July 2016 - Märkte

NTN-SNR entwickelt kabelloses Positionsmesssystem für seine Linearmodule

NTN-SNR hat ein Linearmodul mit einem kabellosen und in die Linearführung integrierten Positionsmesssensor entwickelt. Kompakte Bauweise, einfache Implementierung und der Wegfall störender Kabel…

Lesen Sie den Artikel:
pressrelease
Juni 2016 - Märkte

NTN-SNR's wide product range, modularity and innovations cover all automated movement needs

For the first time, NTN-SNR shall take part in Automatica, the international trade fair for robotics, automation and mechatronics to be held from 21 to 24 June in Munich. NTN-SNR is a major player…

Lesen Sie den Artikel:
pressrelease
Juni 2016 - Gruppe

NTN-SNR is ISO 50001 certified for all its French sites

In January 2016 NTN-SNR obtained ISO 50001 certification for energy efficiency for all its sites in France. The certification acknowledges the work done for several years on reducing NTN-SNR's…

Lesen Sie den Artikel:
pressrelease
Juni 2016 - Gruppe

NTN-SNR extends its lubrication range designed for the single-point lubrication system Ready Booster

NTN-SNR launches Food Chain Oil, its new food-grade oil designed specifically to meet demand from the food-processing and pharmaceutical industries. Food Chain Oil is intended for use with NTN-SNR…

Lesen Sie den Artikel:
pressrelease
Juni 2016 - Gruppe

NTN-SNR is launching in Europe the BBPS 10-100, its kit for extracting deep-groove ball bearings

NTN-SNR is launching in all of its European markets the BBPS 10-100, a kit for extracting deepgroove ball bearings, in order to meet demand for rapid and easy removal of bearings without the risk…

Lesen Sie den Artikel:
pressrelease
Mai 2016 - Märkte

NTN-SNR deploys 2 flagship products for towed agricultural machines

After their launch at the end of last year, NTN-SNR is deploying its offering of built-in hubs and inserts for self-aligning bearing units for all manufacturers of agricultural machines and…

Lesen Sie den Artikel:
pressrelease
Mai 2016 - Gruppe

NTN-SNR mobilized in the fight against forgery

NTN-SNR bearings are prone to copying or forgery. Increasingly sophisticated forgery techniques observed for several years make it virtually impossible for the untrained eye to distinguish non-…

Lesen Sie den Artikel:
pressrelease
Mai 2016 - Innovation

NTN-SNR innovates by proposing reversed tapered bearings at the service of motor vehicle performance

NTN-SNR presents reversed tapered bearings for the motor vehicle industry. This innovation, which was initially designed for gearboxes also has applications in other fields, such as wheels in…

Lesen Sie den Artikel: